Press and News


LAPP Solutions Navigator: Find the Right Cables and Connectors for Your Solar or Warehouse Project

The LAPP Solutions Navigator is a free online tool that shows which LAPP cables and connectors suit each point of a solar or warehouse automation system. You pick an industry,...

Smart Building Cabling Guide: Fieldbus and Ethernet for BMS

Modern building automation uses fieldbus and Ethernet networks to connect devices, controllers and BMS platforms. A building can also use fibre, wireless and dedicated safety cabling, but fieldbus and Ethernet...

How to Read Cable Certification Marks for Regulated Environments: A Selection Guide

The marks on a cable datasheet answer different questions, not the same one. Fire marks split into circuit integrity under fire conditions and flame propagation along the run. Halogen-free and...

Industrial Ethernet Cabling for Cleanrooms and Hygienic Zones: What Changes When the Room Is the Spec

Cleanroom and hygienic-zone Ethernet cabling is a materials decision before it is a data-rate decision. The room's ISO 14644-1 class describes the cleanliness of its air, not the cable, so...

LAPP Harnessing Solutions: Pre-Assembled Connectivity for Hygienic Machine Builds

A hygienic machine build benefits when its cable, connector and gland are assembled and tested together against the machine builder's specified requirements, rather than sourced separately and built up on...

Washdown-Rated Connectors: Specifying EPIC® for Hygienic Food and Beverage Lines

For a food-production line, washdown suitability is a question about the whole connection: housing, seals, cable entry and cleaning duty. IP69 addresses defined ingress conditions, while chemical compatibility and hygienic...

Specifying and Coding EPIC® Rectangular Connectors for a Machine Interface

Specify a rectangular EPIC® connector by matching the housing, insert configuration and contacts to the machine interface. Then select compatible mechanical coding for connections that must not be interchanged and...

Industrial Communication for the Data Centre Facility Layer: BMS, DCIM and Power Monitoring Cabling

Which cable schedule covers the building management system, the DCIM feeds and the power monitoring points? Not the one written for the server floor. A data centre's facility layer runs...

1-8 of 81 articles