Skip to content
LAPP Vietnam
Spend 1.200₫ more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0Cart(0₫)

The Industrial Connectivity Glossary

In the world of industrial automation, the details matter. Understanding the difference between a UL-listed and a CE-marked component, or knowing why you need an IP69K-rated connector, can be the key to a successful, reliable project.

We’ve created this no-nonsense glossary to demystify the key terms you’ll encounter when specifying, buying, and installing high-performance connectivity solutions.

For Field Installers & System Integrators

These are the terms that matter when you’re on-site, getting the job done right the first time.

Term A Simple Definition Why It Matters for Your Project
Bend Radius The minimum radius a cable can be safely bent without damaging the conductors or shielding inside. Respecting the bend radius is crucial. Forcing a cable into a tighter bend than it’s designed for can cause signal loss, data errors, and premature failure, leading to callbacks.
Strain Relief A component, usually part of a cable gland or clamp, that absorbs pulling and bending forces at the connection point. Without proper strain relief, vibrations and accidental tugs will put all the stress directly on the delicate wire terminations inside the connector, which is a primary cause of connection failure.
IP69K Rating The highest Ingress Protection rating. It certifies that a component is completely dust-tight and can withstand high-pressure, high-temperature water jets. This is essential for equipment in food & beverage or pharmaceutical plants that undergo intense daily wash-downs. An IP69K-rated connector ensures zero water ingress, preventing corrosion and short circuits.
Cable Gland A fitting used to securely attach and seal a cable as it enters a piece of equipment or an enclosure. A high-quality cable gland is your first line of defence. It provides strain relief, creates an environmental seal (IP rating), and in the case of EMC glands, grounds the cable shield.
Shield Termination The process of connecting the cable’s metallic shield (braid or foil) to ground, providing a 360° low-impedance path for electrical noise to escape. Doing this correctly is critical for preventing EMI. An improper shield termination renders the best shielded cable useless, leading to phantom errors and system instability.
Crimping Using a specialized tool to mechanically bond a terminal or contact to a wire, creating a secure and gas-tight connection. A good crimp is electrically and mechanically sound. A bad crimp (made with the wrong tool) can lead to high resistance, overheating, or the wire pulling out under vibration.
M12 / M8 Connectors Rugged, circular connectors that are the industry standard for connecting sensors, actuators, and fieldbus devices in industrial automation. Knowing the different codes (e.g., A-code for sensors, D-code for Ethernet) is key to a fast and error-free installation. Using these standardized connectors ensures compatibility and reliability on the factory floor.

For Technical Buyers & Procurement

These are the terms you’ll find on spec sheets and compliance documents that ensure you’re sourcing the right, compliant products for your project.

Term A Simple Definition Why It Matters for Your Project
UL Listed A certification mark from Underwriters Laboratories (UL) indicating that a product meets recognized safety standards for North America. If your machinery is being exported to the US or Canada, having UL-listed components is often a mandatory requirement for customs clearance and site acceptance.
IP Rating (Ingress Protection) A two-digit code that classifies how well a product is sealed against solids (first digit) and liquids (second digit). This is not negotiable. You must match the IP rating to the environment. Specifying an IP67-rated connector for a wet or dusty area prevents premature failure and costly downtime.
CPR Classification (Construction Products Regulation) A European standard (Euroclass) that rates cables on their reaction to fire (e.g., flame spread, smoke, etc.). For projects that require high fire safety standards, such as public buildings or critical infrastructure, specifying a cable with a Cca or B2ca rating ensures you meet modern safety codes.
LSZH (Low-Smoke, Zero-Halogen) A type of cable jacketing material that produces very little smoke and no toxic halogen gases when it burns. In enclosed spaces like tunnels, ships, or office buildings, LSZH cables are critical for safety. They improve visibility during an evacuation and don’t release corrosive gases that can damage sensitive electronics.
ATEX Certified A certification for equipment intended for use in potentially explosive atmospheres (e.g., oil & gas facilities, chemical plants). Sourcing ATEX-certified components is a legal requirement in hazardous zones. It ensures the component will not create a spark that could ignite flammable gases or dust.
AWG vs. mm² Two different systems for measuring wire size. AWG (American Wire Gauge) is common in North America, while mm² is the standard in Europe and Asia. You need to be able to cross-reference these when specifying products. A mismatch could lead to ordering the wrong size cable or connector for the required current capacity.
Total Cost of Ownership (TCO) A financial calculation that includes the purchase price of an asset plus the direct and indirect costs of operation over its entire lifespan. A premium component might have a higher initial price, but it results in a lower TCO by reducing costs associated with downtime, maintenance, and replacement.

For Design Engineers & Specifiers

These are the advanced technical concepts that ensure a system is designed for maximum performance and reliability from the start.

Term A Simple Definition Why It Matters for Your Project
Class 2 Copper Strands A coarser stranding of copper conductors, typically found in cables designed for fixed installation or occasional flexing (e.g., in building wiring). While cost-effective for stationary applications, Class 2 strands are not designed for repeated motion. Using them in cable chains or robotics will lead to early conductor breakage.
Class 5 Copper Strands Finer, more flexible stranding of copper conductors used in cables designed for frequent flexing and movement (e.g., in drag chains). Cables with Class 5 stranding are significantly more durable in dynamic applications, resisting fatigue and breakage from constant bending. Essential for reliable motion.
E-Beam (Electron Beam) Crosslinking A process where cable insulation material is exposed to electron beams, which improves its mechanical strength, temperature resistance, and chemical resistance. This advanced manufacturing technique makes cable jackets and insulations tougher, allowing them to withstand higher temperatures, harsher chemicals, and more abrasion without degrading. It enhances long-term reliability in extreme environments.
Drag Chain Cable A cable specifically designed with high-flexibility conductors and abrasion-resistant jackets to survive millions of bending cycles inside a moving cable chain. Using a standard cable in a drag chain is a guaranteed failure point. A true drag chain cable is essential for the reliability of any ASRS, gantry robot, or moving machine.
Torsion-rated Cable A cable engineered to withstand repeated twisting along its axis (e.g., ±180°/m), which is common in robotic arms and wind turbine loops. Standard cables will fail quickly under torsional stress as the internal conductors bunch up and break. A torsion-rated cable ensures the long-term reliability of rotating machine parts.
Hybrid Cable A composite cable that combines different types of components—such as power, data, and even fibre optics—within a single, rugged jacket. In complex robotics and moving machinery, a hybrid cable saves a huge amount of space, reduces installation time, and simplifies cable management compared to running multiple separate cables.
Single Pair Ethernet (SPE) A new technology that transmits Ethernet data and power over a single twisted pair of wires, ideal for connecting sensors and actuators in IIoT systems. SPE allows you to extend the reach of your Ethernet network deep into the field with simpler, lighter, and more cost-effective cabling, breaking down old fieldbus communication barriers.
EMC (Electromagnetic Compatibility) The ability of a system to function correctly in its electromagnetic environment without generating or being affected by electrical noise. Achieving good EMC is a system-level goal. It requires a combination of shielded cables, proper grounding, and EMC-rated glands and connectors to prevent interference and ensure reliable operation.
MICE Rating A system for classifying the harshness of an industrial environment based on four factors: Mechanical, Ingress, Climatic/Chemical, and Electromagnetic. Using the MICE framework helps you specify the exact level of robustness needed for your cables and connectors, ensuring you don’t over-engineer (and overpay) or under-engineer (and risk failure).

For Facility & Maintenance Managers

These are the terms focused on long-term reliability, safety, and keeping the plant running smoothly after installation.

Term A Simple Definition Why It Matters for Your Project
Insulation Resistance Test A preventive maintenance test where a high DC voltage (“Megger test”) is applied to a cable to measure the integrity of its insulation. A low reading indicates that a cable’s insulation is degrading, possibly due to moisture or physical damage. This test helps you find and replace failing cables before they cause a short circuit or a safety hazard.
Thermal Imaging (Thermography) The use of an infrared camera to scan electrical panels, motors, and connections to find abnormally hot spots. A hot spot is a clear sign of a problem, such as a loose connection or an overloaded circuit. Regular thermal scans are a powerful, non-invasive way to predict failures before they happen.