Skip to content
LAPP Vietnam

One Cable, More Control: A Practical Guide to Industrial PoE

A security camera at your warehouse loading bay drops its connection every time a forklift’s VFD spins up. The video feed freezes. A tech spends an hour tracing the fault, assuming the camera or switch is dead.

The problem isn’t the camera. It’s electrical “noise” from the forklift’s motor drive coupling onto a cheap, unshielded Ethernet cable. The fix wasn’t a new camera; it was specifying the right cable for the job.

Power over Ethernet (PoE) is a powerful deployment model. It promises one-cable simplicity for power and data. But in a “noisy” industrial environment like a warehouse or smart factory, a successful PoE rollout requires an industrial system approach.

This guide helps operations and IT leaders decide where PoE fits, what its limits are, and the three key considerations that ensure a reliable rollout.

What PoE Solves (And What It Doesn’t)

In an office, PoE is a simple convenience. In a warehouse or smart building, it’s a strategic tool.

The Key Advantages:

  • Single-Cable Install: Cuts installation labour and material costs in half. This makes “Moves, Adds, and Changes” (MACs) fast and simple.
  • Centralised Power: Critical edge devices (cameras, access points, sensors) can be backed up from a single, central Uninterruptible Power Supply (UPS).
  • Remote Control: A non-responsive device can be remotely power-cycled (rebooted) from the IT room without needing a scissor lift.

The PoE Device Matrix: Where Does It Fit?

PoE is perfect for low-to-medium-power edge devices. It is not for high-power industrial machinery.

Device Type PoE Fit? Why?
IP Cameras (Fixed) YES (PoE+) The “killer app” for PoE. Perfect for easy mounting and central UPS.
Wi-Fi 6/6E Access Points YES (PoE+) Essential for reliable roaming. Easy to install on ceilings.
Access Control / Intercoms YES (PoE) Low power, critical function. PoE simplifies wiring through door frames.
IoT / Occupancy Sensors YES (PoE) Ideal for low-power “smart building” data collection nodes.
High-Power PTZ Cameras MAYBE (PoE++) These “PoE++” devices (60W-90W) can quickly exhaust a switch’s total power budget.
Smart Lighting MAYBE Yes for low-voltage PoE nodes, but often not for high-lumen fixtures.
Motors, Drives, Heaters NO These are high-power devices requiring dedicated power cabling.
Large HMIs / PCs NO These devices typically exceed the 90W maximum of PoE.

The Limitations: There are three key limitations to consider with any PoE system:

  • Distance: 100 metres (328 feet) for the total cable channel.
  • Power: The switch or injector has a total power budget that it must share across all ports.
  • The Environment: PoE does not make a cable immune to heat, moisture, or electrical noise (EMI).

3 Key Planning Considerations for a Reliable PoE Rollout

Success with industrial PoE comes down to three key planning choices.

1. Topology (Endspan vs. Midspan)

This is the “how” of power delivery.

  • Endspan (PoE Switch): A network switch that has PoE built directly into its ports.
    • Best for: New builds and clean cabinet designs. It’s one device to manage and allows for monitoring power per port.
  • Midspan (PoE Injector): A separate device that sits between a non-PoE switch and the end device, “injecting” power onto the data cable.
    • Best for: Retrofits. This allows adding a few PoE devices without replacing an entire core switch.

In a large ASEAN warehouse, placing smaller PoE switches (Endspans) in local cabinets closer to the devices is often smarter than running hundreds of long cables back to one central room.

2. Power Budgeting (A Critical Calculation)

A PoE switch is not an infinite power source. The planning process involves adding up the maximum power draw for every device intended for connection. This total is then compared to the switch’s total PoE budget (e.g., 370W).

A best practice is to leave 20-30% headroom and not “redline” the power budget. A switch running at 100% capacity will run hot and be unstable. The power levels for devices (PoE, PoE+, PoE++) are all defined by the IEEE 802.3 standard.

The ASEAN Angle (Heat): In a hot, humid warehouse, bundled cables running high-wattage PoE get even hotter. This heat increases the cable’s resistance, wastes power, and can degrade the cable jacket. High-temperature-rated cables are a wise choice, as is avoiding massive, tight bundles.

3. The Cabling System (Industrial vs. Office)

This is the most common failure point. An office-grade, unshielded (UTP) cable was never designed to survive next to a 3-phase motor.

The Problem: Unshielded cable acts as an antenna. It absorbs all the electrical “noise” (EMI) from VFDs, motors, and fluorescent lighting, leading to dropped packets, connection freezes, and “ghost” faults.

The Solution: An industrial-grade, shielded cabling system is the common solution.

  • The Cable: This system typically includes a shielded Cat6A cable like LAPP ETHERLINE®. Its robust jacket (e.g., PUR) resists oil and abrasion, and the shield protects the data.
  • The Termination: A shield is useless if not grounded. A “pigtail” twist-and-tape termination is a high-impedance path that reflects noise. A SKINTOP® EMC Gland at the cabinet entry provides a low-impedance, 360° connection that safely drains noise to ground.
  • The Protection: In harsh areas, cables are often run in conduits and terminated with robust, sealed EPIC® industrial connectors instead of fragile RJ45 clips.
  • The Surge Risk: In a large warehouse with long cable runs or outdoor-mounted cameras, lightning-induced surges are a real threat. In these cases, Ethernet surge protectors are a common solution to protect the switch and the camera.

The Bottom Line: PoE Is a System, Not a Cable

PoE is a deployment model that simplifies the edge, centralises the UPS, and provides remote control. But to gain those benefits, success depends on respecting the industrial environment.

The most reliable rollouts treat PoE as a complete system. They start with a smart plan (topology and power budget) and finish with industrial-grade components: shielded cables, 360° EMC grounding, and robust connectors.

To make this fast and repeatable, especially across multiple sites, many operations use pre-terminated assemblies and kitted cabinets. This moves the high-skill termination and testing work from a scissor lift on a busy site floor into a controlled, clean workshop.

Frequently Asked Questions (FAQ)

When should 24V DC power be used instead of PoE?

24V DC is a great fit for simple, non-data devices like basic proximity sensors, stack lights, or solenoid valves. PoE is the ideal choice for data-heavy devices (cameras, Wi-Fi, HMIs) where the “single-cable” advantage and network connectivity are the primary benefits.

Is shielded “Industrial Ethernet” cable really that different?

Yes. The differences are significant. It’s not just the shield. The jacket material (like PUR) offers high resistance to oils, chemicals, and abrasion. The construction is often designed to withstand vibration or even flexing (in the case of ETHERLINE® FD cables), which would destroy an office-grade cable in weeks.

Will my PoE cables really get hot?

Yes. When running high-power PoE++ (60W-90W), the power dissipates as heat. In a tight bundle of 24 or 48 cables, this heat builds up, increasing resistance and power loss. It’s critical to use cables rated for higher temperatures (e.g., 75°C or 90°C) and follow installation guidelines for bundle size.