Skip to content
LAPP Vietnam

LAPP Connector Solutions for Industrial and Data Centre Builds in ASEAN

A LAPP connector solution is the combination of EPIC® industrial connectors, SKINTOP® cable glands, and LAPP-cable-and-connector pre-assembly through LAPP Harnessing Solutions, delivered as a coordinated specification rather than three separately-sourced layers. Connectors are manufactured at LAPP facilities including LAPP Connectors Dongguan (LCD), and LAPP SEA holds regional stock across ASEAN markets so specifiers scope cable and connector together with one engineering contact. The benefit is a single tolerance reference at the cable-connector interface, one warranty path when a fault appears in the field, and predictable lead times against confirmed regional stock.

For specifying engineers, procurement leads, and OEM electrical designers across ASEAN, the recurring problem with connector sourcing is not spec complexity. It is accountability fragmentation. A factory harness fails in the field, the cable came from one supplier, the connector housing from a second, the gland from a third. Each party points at the other. This guide explains what a LAPP connector solution actually covers, how to specify EPIC®, SKINTOP®, and harnessed assemblies together, and where the LCD manufacturing context matters for regional supply.

What Counts as a LAPP Connector Solution, and Why Does It Matter?

The short answer: cables, connectors, and glands from one engineering programme.

LAPP designs and manufactures EPIC® industrial connectors and SKINTOP® cable glands in-house, and it supplies the ÖLFLEX® and ETHERLINE® cable families that terminate into them. When you specify a LAPP connector solution, you are working from one tolerance document, one technical support line, and one warranty path when something fails. That is the practical meaning of “single-source accountability” in this context.

The EPIC® range covers the full connector envelope for industrial automation, machine building, packaging, robotics, intralogistics, EV charging, and AI data centre applications:

EPIC® Signal connectors for control and sensor wiring, available in circular and rectangular housings with pin counts from 3 to 144 contacts

EPIC® Power connectors for power-feed and motor connections, including high-voltage, high-current power variants

EPIC® Harnessing-ready assemblies pre-wired through LAPP Harnessing Solutions, where the cable-to-connector tolerance is built in at the factory

SKINTOP® cable glands, sized to the cable outer diameter and rated for the installation environment, including variants for dry-room, solvent-adjacent, and IP68-required zones

Specifying these three layers as a single programme is not the only approach. But it eliminates the tolerance-matching problem that surfaces when a third-party connector housing is bolted onto LAPP cable by a sub-contracted workshop.

How Do You Specify EPIC®, SKINTOP®, and Harnessed Assemblies Together?

The specification sequence has four layers.

First, define the cable. ÖLFLEX® for power and control, ETHERLINE® for industrial Ethernet, UNITRONIC® for instrumentation and bus. The cable outer diameter, conductor count, and jacket material set the constraints for everything downstream.

Second, select the EPIC® connector housing to match the current, voltage, and contact-count requirements of the connection. Circular EPIC® housings (M8 to M23 and larger) cover sensor and drive connections. Rectangular housings (H-BE, H-B, H-A series) handle higher pin counts and heavier power feeds. For each, LAPP publishes the compatible cable outer diameter range.

Third, specify the SKINTOP® cable gland. Gland size is a function of cable OD. Material selection depends on the installation zone: brass for general industrial, stainless steel for food processing and offshore, polymer variants for weight-sensitive or corrosive environments. IP rating on the assembled gland holds when the cable OD is within the gland’s specified range.

Fourth, decide whether to spec factory assembly through LAPP Harnessing Solutions or site assembly. Factory harnessing wins on tested continuity and first-build cost-per-unit at volume. Field-attachable wins on schedule flexibility and field-repair turnaround. The Integrated Connectivity blog from March covers the make-versus-buy logic in detail.

The practical output of this sequence is a cable-and-connector schedule where every SKU is on the same LAPP datasheet envelope and the LAPP SEA team can confirm regional stock before the BOM is finalised.

Where LAPP Connectors Are Made: The LCD Manufacturing Context for ASEAN

LAPP Connectors Dongguan, or LCD, is the LAPP manufacturing facility in Dongguan, China that produces EPIC® industrial connectors for the ASEAN supply chain. It is not a product category name. It is the factory address behind the regional connector stock that LAPP SEA holds across Singapore, Malaysia, Thailand, Vietnam, Indonesia, and the Philippines.

The significance for an ASEAN specifier is lead time and continuity. EPIC® connectors supplied through LAPP SEA draw on LCD production with confirmed regional stockholding, which means the connector BOM locks in at the same time as the cable schedule rather than after a separate Europe-direct procurement cycle.

For data centre and AI infrastructure builds in the region, this matters because project timelines are compressing. Hyperscale and colocation builds that historically ran on longer lead times are increasingly being committed and delivered on compressed schedules. A cable-and-connector BOM that can be confirmed against confirmed regional stock removes one variable from the critical path.

When Does a Single-Source Connector Solution Outperform Multi-Vendor Sourcing?

Multi-vendor sourcing has a place. If a project already has a connector standard locked in by the machine OEM, matching the cable to the existing housing is the right call. Single-source is not the only correct answer.

Single-source consistently outperforms multi-vendor sourcing in four scenarios:

Accountability gaps are a concern. On large plant builds where sub-contracted electrical workshops do the harness assembly, a three-vendor BOM (cable, connector, gland from different suppliers) creates no clear owner when a field fault appears. Single-source puts the technical responsibility on one party.

Cable-connector interface risk is high. EPIC® housings are dimensioned against ÖLFLEX® and ETHERLINE® cable ODs. Third-party cable that falls outside the rated range can compromise the gland seal or the strain-relief performance.

Regional lead time is a constraint. LCD-to-LAPP SEA stock is a shorter pipeline than Europe-direct procurement for most ASEAN applications.

High-cycling applications. In EV charging, robotics, and automated assembly, connectors cycle frequently. The EPIC® Connectors Comparison blog documents the mating-cycle performance data for the range.

The honest framing: single-source is not about exclusivity. It is about reducing the number of tolerance mismatches and warranty grey areas in a harness assembly. For multi-site builds and AI data centre deployments where standardisation across racks matters, it also simplifies BOM documentation and long-term procurement.

Talk to Our Engineers

LAPP designs and manufactures cables AND connectors under one engineering programme. LAPP SEA stocks EPIC®, SKINTOP®, and the matching ÖLFLEX® and ETHERLINE® cable families across ASEAN, with the LCD manufacturing pipeline behind regional supply. Whether you are scoping a single machine harness or a full data centre cable schedule, our connectivity specialists can confirm the cable-connector pairing against your application requirements. Talk to our engineers at https://e.lapp.com/apac/contact to see how LAPP serves your industry.