Skip to content
LAPP Vietnam

Field-Attachable Industrial Connectors: Faster Intralogistics Deployments

When should you specify a field-attachable industrial connector instead of a factory-crimped harness? Specify a field-attachable connector, typically an EPIC® screw-terminated housing or an M12 field-wireable variant, when on-site termination flexibility matters more than the repeatability of a factory-assembled cable. Field-attachable is the right call for intralogistics commissioning where layouts shift late, for AGV and AMR field service where downtime depends on how fast a damaged cable can be replaced, and for any deployment where the lead time on a factory-assembled harness would push the project past its commit date.

For site commissioning engineers, intralogistics maintenance leads, and OEM electrical designers across ASEAN, the framing that fails in practice is treating field-attachable connectors as the cheap shortcut to a factory-crimped harness. They are not a shortcut. They are a different tool for a different job. LAPP makes the cable AND the connector AND the cable gland under one engineering programme, and the EPIC® screw-terminated and M12 field-wireable ranges sit alongside factory harnessing as parts of the same toolkit. This guide walks through when field-attachable is the right call, when it is the wrong call, and how the EPIC® range fits the intralogistics specification context.

What Is a Field-Attachable Connector and When Should You Specify One?

A field-attachable (also called field-wireable) connector is a housing designed for the installer to terminate cable on site rather than receive a pre-terminated assembly from a factory. The housing accepts a defined range of cable diameters, the conductors land on screw terminals or insulation-displacement contacts, and the assembly is closed with a strain relief and gland that can maintain the rated IP protection when assembled to specification.

The decision to specify field-attachable comes down to four questions:

  • Will the layout shift after the cable is ordered?
  • Does the team need to replace a damaged cable in service without waiting on a factory lead time?
  • Are cable lengths variable enough that pre-cutting to spec is impractical?
  • Is the install team trained and equipped to terminate the connector to specification?

If three of those four answer yes, field-attachable is the right call. If three answer no, factory-crimped harnessing through LAPP Harnessing Solutions is usually the better fit.

How Do Field-Wireable Variants Compare to Factory-Crimped Harnesses?

Factory-crimped harnesses win on first-build cost-per-unit, on tested electrical continuity, and on repeatability across production batches. They lose on schedule flexibility, on field-replacement turnaround, and on the per-channel termination cost when run lengths change late.

Field-attachable connectors invert the trade-off. They win on schedule (the connector is on the shelf and the cable cuts to length), on field repair (repairs can often be handled on site without waiting for a replacement pre-terminated harness), and on configuration changes after the initial install. They lose on first-build labour cost (each termination takes minutes rather than coming pre-tested), on the consistency that a factory crimp delivers, and on training overhead (the install team has to terminate to specification).

The honest comparison is the lifecycle cost across first-build plus expected field service. For a one-off build with stable layout, factory-crimped wins. For a fleet of AGVs with a five-year service plan and a maintenance team on standby, field-attachable wins. For most intralogistics projects, the right answer is a mix: factory-crimped on the trunk runs that will not change, field-attachable at the end-effector, sensor, and replaceable-cable interfaces.

The Mar W1 EPIC Industrial Connectors Comparison blog walks the EPIC connector range in more depth, which is the foundation for the field-attachable variants this guide covers.

EPIC® Screw-Terminated and M12 Field-Wireable: What LAPP Carries for Site Assembly

The EPIC® range covers the heavy-duty side of field assembly. Rectangular housings (the H-B and H-A series) accept modular inserts and terminate on screw or crimp contacts that the installer can land in the field. The housings ship with a defined gland range and strain-relief geometry so that the assembled connector preserves its IP rating when wired correctly.

The M12 field-wireable variants cover the circular side. M12 D-coded for 100 Mbit/s PROFINET, M12 X-coded for gigabit Ethernet, and additional M12 codings for sensor power and signal are available in field-attachable bodies, with application suitability depending on the protocol and the power requirements of the device. The cable gland and strain-relief specification on the M12 body sets the cable-diameter range and the IP rating the assembled connector will hold.

The matching SKINTOP® cable glands handle the bulkhead entry where the cable transitions from the cable tray or drag chain into the enclosure. Specifying the cable, the connector, and the gland from one engineering programme means that the cable diameter, the gland clamping range, and the connector strain relief all line up without on-site improvisation.

When Is Field Termination the Wrong Call?

Three patterns make field termination the wrong call.

First, when the install team cannot terminate to the published specification. Field-attachable IP ratings are conditional on correct strip length, conductor seating, gland torque, and strain-relief assembly. Without the right tooling and training, the assembled connector typically drops below its advertised IP rating at the cable entry and the warranty expectations follow.

Second, when the channel needs to be tested before energising. Factory-assembled harnesses can be supplied with documented continuity and high-pot test reports, depending on the assembly specification ordered. A field-attached connector is tested at install, which means the install team needs the test equipment and the procedure documented. For safety-critical or high-availability runs, the factory-crimped path keeps the test report in the supplier’s hands.

Third, when the run is high-volume and identical. A fleet of fifty identical AGVs with identical dressing packs is a strong factory-harness case. The per-unit cost difference compounds across the fleet and the QA repeatability is hard to match in the field. The LAPP SEA intralogistics hub covers the broader intralogistics specification context for these decisions, and the May W2 cable selection piece walks the duty-cycle side that pairs with the connector decision.

Talk to Our Engineers

Field-attachable connector specification is both a technical connector-selection decision and a procurement strategy choice (factory vs field, by section of the install). The LAPP SEA team can sit with your commissioning, field service, and procurement teams and put a connector strategy on the BoM before the first cable ships.

Talk to our engineers about your field-attachable connector specification, an existing-fleet field-service plan, or any specific EPIC® or M12 field-wireable question.